Image Output

Community Manager Community Manager
Community Manager

In Femap you can generate a picture of the graphics screen at a resolution that is higher than the actual screen resolution, which means that you can create images with a greatly improved picture quality. You can have Femap automatically query your printer to establish the maximum allowable image resolution or specify the desired resolution or scale factor with which to copy or save the image. The image size can be determined by specifying a scale factor, or you can explicitly define the image pixel dimensions. You can also control other factors such as pen width and logo and background scaling.

 

08_01.jpg

 

Control of graphical output can be found in File | Preferences menu, then select Views in the Preferences dialog.

 

08_02.jpg

 

 

 

(view in My Videos)