Cancel
Showing results for 
Search instead for 
Did you mean: 

Multiple Legends for Postview Overlays

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

In many multi-physics applications, it is required to review multiple results on the same display.  One example is the vibro-acoustic analysis, where structural result (vibration) and acoustic result (sound pressure) are usually superimposed on the same display, each with its own color legends.  This can be easily setup in Simcenter 3D.   

 

After loading the result file, go to File -> Preferences -> Post Processing.  Toggle on the option Multiple Legends for Postview Overlays and OK

 

V1.png

 

In the Post Processing Navigator, Plot the Structural displacement first (order is not important), and then use the Overlay option to superimpose the pressure to the existing display

 

V2.png

 

Now you should see both results are diplayed on the same plot, two color legends are automatically separated.  You can use the tool Edit in Graphics (in tab Results) to manually adjust the locations of these color legends if necessary.

 

 V3.png