Cancel
Showing results for 
Search instead for 
Did you mean: 

How to increase the Increment in the result

Experimenter
Experimenter

 Dear All,

 

How can I increase the INCREMENT in the result after simulated model?

 

In the attachment, it showed the maximum of Increment is 12, but I wish to make the load press the structure till the end of the tube.

 

Is that available in NX? If yes, how to make it?

 

Thank you.

3 REPLIES

Re: How to increase the Increment in the result

Gears Phenom Gears Phenom
Gears Phenom

you end up with 12 increment because that's what you requested!

to crush the tube then you need to apply a much larger force but one usually use forced displacement for such problem. You will most likely end up with analysis "difficulty" becuase of self-contact, large stress/strain, etc

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: How to increase the Increment in the result

Experimenter
Experimenter

Thanks for your advice...
So, what should I do? does any guidance steps or demo video available to refer? Because I not familiar with the

Currently, I'm using NX10 on academic purpose, and I'm not familiar with this software yet. Hope somebody can help me...

Re: How to increase the Increment in the result

Gears Phenom Gears Phenom
Gears Phenom

if not familar with the software then I can only recommend starting with an (easy) problem. Starting with the problem described is not the easiest. No even sure if an academic licence can handle such problem - don't knwo the limitatin of such licence

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)