Cancel
Showing results for 
Search instead for 
Did you mean: 

NX ADVANCED SIMULATION "DYNAMIC" PRESS FIT

Creator
Creator

Hi to everybody :-)
I am new of this forum but I hope that someone can help me. I would to study a dynamic deformation of hole and pin when the last one go inside. aaaaaa.jpg

bbbbbb.jpg

 

It is possible with Non Linear Advanced solution to study it? My target is to see how the pin and the hole deform.

I created a mesh for both of 0.1 size, I assigned the material ( plastic ), I fixed the hole and I assigned a enforced displacement of 0,5mm to the pin to allow the traslation. How can I go on now? I have to create a "mesh meting" between them? According to you can I see a "dynamic" deformation of hole and pin´s mesh during taslation of the pin.

Thank you very much  if you give me some suggestions.