Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Nastran on HPUX C8000 with 4 processors.

Not applicable

Is someone setup for Multi-processors machine ?.
Do I need special license for Nx-nastran ? software ?.
Thanks.
Lan
2 REPLIES

Re: NX Nastran on HPUX C8000 with 4 processors.

Not applicable

Hello Lan,
Did you ever get a response to your question?
Mark

"Lan Nguyen" wrote:
>
>Is someone setup for Multi-processors machine ?.
>Do I need special license for Nx-nastran ? software ?.
>
>Thanks.
>
>Lan

Re: NX Nastran on HPUX C8000 with 4 processors.

Not applicable

"Lan Nguyen" wrote:
>
>Is someone setup for Multi-processors machine ?.
>Do I need special license for Nx-nastran ? software ?.
>
>Thanks.
>
>Lan

I am running XP (SP2) on a PC with two dual core processors. When I set the number
of processors to 4 in the analysis case dialog boxes, all 4 processors are used
for the analysis. I can only suggest you just try it.
Best of luck,
Carlton.