Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Normal mode shape display in phase

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,

from the modal analysis I have normal frequency and mode. The mode (shape) is mostly displayed as displacement, e.g. for simple bar it is bending. And I want to display it in opposite direction as default - in opposite phase. How to get it? Is it a setting of NX Nastran solution or just function of Simcenter post process?

Juraj

3 REPLIES

Re: Normal mode shape display in phase

Gears Phenom Gears Phenom
Gears Phenom

animate the mode shape and select the frame in which the part is the "position" you want perhaps

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Normal mode shape display in phase

Legend
Legend

Setting the deformation scale of the post view to a negative value will flip the phase of the deformed shape. I do not know how to set this as a default so you may need to create a post processing template to quickly apply the format.

Re: Normal mode shape display in phase

Siemens Phenom Siemens Phenom
Siemens Phenom

Specify a negative scale factor on the deformation dialog

 

Deformation =10% of model (Default):

ModeDisp+10.png

 

Deformation = -10%:

 ModeDisp-10.png