Cancel
Showing results for 
Search instead for 
Did you mean: 

VISUALIZE ON FEMAP DEATH ELEMENTS

Creator
Creator

Hello,

 

I am doing a nonlinear static analysis with SOL601. I have set XTCURVE=0, so when the elements reach the maximum stress they are not more considered in the analysis. How I can check on FEMAP if the elements "die"?which one and when?

Thank you

1 REPLY

Re: VISUALIZE ON FEMAP DEATH ELEMENTS

Siemens Phenom Siemens Phenom
Siemens Phenom

When the element "ruptures", it no longer has results available in Femap. So make sure you request output at enough increments that you can identify at what load level the element results become zero.See the following screen shots below. The first is load level .50 and the yield stress is set to 30000, the second the load has increased to .56 and the element no longer has results.

2017-09-06 09_38_33-Femap with NX Nastran - [rupture.modfem _ Untitled].pngload level =.502017-09-06 09_39_45-Femap with NX Nastran - [rupture.modfem _ Untitled].pngload level = .56, stress exceeded 30000

 

Hope this helps,

Joe