Showing results for 
Search instead for 
Did you mean: 

Warning Message in NX Nastran while using Bolted Connections



Please look at the below image that alone describes the warning message.


I am solving SOL 101 Linear statics problem of Spare Wheel Bracket with 2.5 g .

I have used Bolted Connections and Contacts for defining the connections.

While doing Model Check up i end up with the below highlighted warning.

How could i rectify the below because of what i guess it is not able to solve the problem?

The fatal warning that i get is also attached.


Suggestions Please.


Fatal .PNGWarning.PNG