Cancel
Showing results for 
Search instead for 
Did you mean: 

Workaround for Varying Distance and constant Temperature

Hi,

I am using NX-9. I need to simulate for the Varying distance and the temperature should be constant at the same time. You can take an example as of welding.

 

I have attached image. the bottom is the plate with ambient temperature. whereas the rod(heat Source) is in contact with the plate and moves on the plate in the X-direction.

 

How to workaround this problem, kindly help me to resolve this issue. I am not sure if it is possible by creating fields. if yes how to create field for this kind of scenario.

 

Similar to this video

Link - https://www.youtube.com/watch?v=UfcJp215gs0

SLS.JPG

 

Regards,

Piyush

 

 

1 REPLY

Re: Workaround for Varying Distance and constant Temperature

Hi,
Please help me in this issue.