Cancel
Showing results for 
Search instead for 
Did you mean: 

Anchor chain simulation for a trebuchet

Experimenter
Experimenter

Hey there, the last view weeks I have been working on a simulation of a modern trebuchet (medieval artillery weapon). I now have a design that uses a weight on a chain and the chain is attached to rotating arms on the trebuchet. I have been breaking my head over finding a proper way to simulate the chain. I have made a test simulation of a small chain (13 links) using 3D-contacts between all the adjoining links. The simulation takes about 1.25 seconds however rendering the simulation takes 45 minutes on my laptop (because of the 3D-contacts I assume). Since I want to use a (3 times) longer chain, I've been trying to find another way of going about this simulation.  I hope somebody can help me to either find another way than 3D-contacts or a smarter way to go about using 3D-contacts. I hope I am on the right forum for this question else please let me know. If you need a better visualization of what I am trying to accomplish I also uploaded an animation of the rotation of the trebuchet. Thanks in advance.

Kind regards

1 REPLY 1

Re: Anchor chain simulation for a trebuchet

Phenom
Phenom

Hi,

I guess the first way to simulate is without solid and without contact.

A chain can be seen as an assembly of (rigid or elastic) beams or rods connected with translational DOFs and with one or two rotational DOFs as a joint like an hinge. Try to keep it simple.

Best wishes, Michael

| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11 | engelke engineering art GmbH, Germany
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution".

Kick Off (2015-09-14)On the Map (2016-10-21)1st Gear 2018 (2018-02-19)To the Rescue (25, ‎2018-02-24)5th Birthday! (2018-02-25)Popular (100, ‎2018-10-30)Prolific (100, 2019-02-27)Philosopher (500, ‎2019-02-28)