Cancel
Showing results for 
Search instead for 
Did you mean: 

Block UI Styler error with expressions and buttons

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Dear All,

 

I am having some issues with Block UI Styler. I am using Simcenter 1872 and my easy goal is to create a GUI like this :

 GuiExample.jpg

(only containing an expression and a button)

 

I have no problem if I try to display that on a not empty part, but if I try to do the same with un empty part (e.g. the one created by default with File->new-> Model) what is shown is the following error message

error.png

 

Which seems to be linked to the following error message in the log File:log.jpg

 

I am using the C++ code generated by Block UI styler itself and to retrieve the dlx I am using the UGII_USER_DIR environment variable.

 

Someone has any ideas why this error occurs and what I can do  to fix it?

 

 

Thanks in advance

1 REPLY

Re: Block UI Styler error with expressions and buttons

Gears Phenom Gears Phenom
Gears Phenom

post your question to https://community.plm.automation.siemens.com/t5/NX-Programming-Customization-Forum/bd-p/NX-Programmi...

you'll have a better chance of a response

Production: NX.CAE 9.0.3.4, NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)