Cancel
Showing results for 
Search instead for 
Did you mean: 

CBAR - elastic axis & gravity axis?

Gears Valued Contributor Gears Valued Contributor
Gears Valued Contributor

Dear people,

 

please see the attached image from this source: Element Library Reference.

CBAR.PNG

1) What is the elastic axis? If it is the same as the neutral axis, I will not need an explanation.

 

2) But then, do neutral axis and gravity axis not coincide all the time? If not, do you have an example of a cross-section?

 

3) If the elastic axis is different from the neutral axis, please explain it + example of a cross-section.

 

Kind regards.

3 REPLIES 3

Re: CBAR - elastic axis & gravity axis?

Genius
Genius

Hi,

 

The elastic neutral axis is at the area centre. For pure bending the longitudinal stress at that point  is zero by definition. To answer your question I think the "elastic axis" is short for "elastic neutral axis".

 

The plastic neutral axis is  generally offset from the area centre for non-symmetrical sections. Note also that the term "neutral axis" sometimes also is used to define the point with zero longitudinal stress when having combined bending and axial force. Care should therefore be paid when using the "neutral axis" term.

 

The gravity axis definition is used for the CBEAM element, allowing you to to define non structural mass offset from the area centre. This additional axis definition is not possible for the CBAR element.

 

This is my understanding. Please correct me if I am wrong.

 

 

BR

Geir Olav Guddal

 

 

Re: CBAR - elastic axis & gravity axis?

Gears Valued Contributor Gears Valued Contributor
Gears Valued Contributor

Thanks for your reply.

 

"allowing you to to define non structural mass offset from the area centre."

 

Why and when would you apply such an offset?

Re: CBAR - elastic axis & gravity axis?

Genius
Genius

Hi,

One example could be the mass of insulation below the beam for instance, or maybe the mass of wooden planking resting on top of the beam?
I think this option can be useful from time to time. One obvious solution depending on correct mass is the calculation of eigen frequencies.

 

Best regards

Geir Olav