CWELD in NX 11 Advanced Simulation

Creator
Creator

Hi,

 

I am looking to create CWELD elements using NX 11 advanced simulation. Whilst this function is available within the help menu I cannot find the operations to create this within the .fem file. Is it possible to confirm whether the function to create CWELD elements is available in version 11, and if so how this is possible?

 

Many thanks!

2 REPLIES 2

Re: CWELD in NX 11 Advanced Simulation

Siemens Genius Siemens Genius
Siemens Genius

Hi

 

This is available when a FEM is active.  Go to the Connections group in the Home ribbon > More > CFAST/CWELD.

 

Alternatively type CWELD in the Command Finder and it should be the only hit.

 

Regards

Joe

Re: CWELD in NX 11 Advanced Simulation

Creator
Creator

Thanks Joe,

 

I did not have the .fem fully active i.e. status set to both "displayed & work". I can now see the CWELD options.

 

Many thanks,

Tom