Can NX v12 Part be used in Simcenter3D v11 for analysis

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Can a NX V12 parametric .part file be used in Simcenter 3D V11 for Analysis, Will the part file be compatable with Simcenter3D modelling.

 

Or should NX and Simcenter3D be same versions.

 

3 REPLIES 3
Highlighted

Re: Can NX v12 Part be used in Simcenter3D v11 for analysis

Siemens Legend Siemens Legend
Siemens Legend
Hi Sanjay,

Simcenter 3D is based on the NX modeling kernel so you cannot read a part fule of a newer NX release to Simcenter 3D.

You coud export a Paradolid from NX12 and read to SC11 or use Step or JT. However you will loose the part history in that case.

If you run NX12 and have the licenses for Simcenter 3D you can directly switch to PrePost in NX. You don‘t need a separate Simcenter 3D installation.

Typically the use cases I know of is that customers would like to use a more recent version of Simcenter than they use in CAD and that is of course possible.

Best regards
Boris

Re: Can NX v12 Part be used in Simcenter3D v11 for analysis

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

Should NX license and SC license be integrated to one license to have Pre post and solver in Nx?

 

Re: Can NX v12 Part be used in Simcenter3D v11 for analysis

Siemens Legend Siemens Legend
Siemens Legend
Typically if you have oneSold To that should be the case.
The installation of NX has the Pre Post functionality inside. Please try
Application —> PrePost

Regards
Boris