Cancel
Showing results for 
Search instead for 
Did you mean: 

Copying which Post View Templates are loaded to new SC installation

Legend
Legend

Is there a way of copying over my list of loaded Post View Templates from one installation of Simcenter to another? Every time I install a new version of SC, or install the same version on a new PC, I always have to manually load in all my Post View Templates.

2 REPLIES

Re: Copying which Post View Templates are loaded to new SC installation

Siemens Phenom Siemens Phenom
Siemens Phenom

Post View Templates can be stored in a central location defined by the UGII_CAE_POST_TEMPLATE_USER_DIR user variable.

 

See Post view templates in the online help. In particular, the Create and manage post view templates article.

 

 

Re: Copying which Post View Templates are loaded to new SC installation

Legend
Legend

@JimB,

 

I was following all the info I could in all those help files (e.g., defining the environment variable, updating customer defaults) and was getting frustrated that none of my post view templates would automatically load. Then I figured out that the only templates in the directory that are automatically loaded are those whose filename starts with "NXPostTemplate_".

 

The devil's in the details they always say.

 

 

Thanks for the pointers,

 

James