Cancel
Showing results for 
Search instead for 
Did you mean: 

Export PNG with check of existence

Gears Phenom Gears Phenom
Gears Phenom

Hi Experts,

 

if I want to export a capture of the graphic window via PNG

 

=> FILE => EXPORT => PNG

 

NX does not check if the file I will create already exists.

I thought its an operating system function which garantees that an existing file will NOT replace automatically.

 

Can I active it in NX may be via customer defaults or is there a script anywhere to do so?

 

Any suggestions are welcome. 

 

Best regards.

Michael

_____________________________________________________
| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11 | engelke engineering art GmbH, Germany
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution".