Cancel
Showing results for 
Search instead for 
Did you mean: 

Failure to Export to MSC Nastran

Experimenter
Experimenter

My office has licenses for Simcenter (SC12500). We use NX 8.5 and NX 12.0.

 

When I open a new model, associate it with a master part, and create a mesh in 8.5, I'm able to export it to MSC Nastran.

 

When I do the exact same thing in 12, I get an error that reads: "Nastran export: no license". Has anyone seen this behavior? Did Siemens change that way it licenses the MSC Nastran translator?

 

Thanks,

Ken

2 REPLIES 2

Re: Failure to Export to MSC Nastran

Phenom
Phenom

Hi Ken,

only as an idea: Check the licence type in "solver parameters" of simulation. Maybe that's the reason. We had a similar problem and didn't realize, that in one case license type was "Desktop" by default and in another case it was "Enterprise". We have only "Desktop" license so it works only in the first case automatically. After switching to License Type "Desktop" in the second case everything was  good.

I hope, it helps. Best wishes, Michael

| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11 | engelke engineering art GmbH, Germany
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution".

Kick Off (2015-09-14)On the Map (2016-10-21)1st Gear 2018 (2018-02-19)To the Rescue (25, ‎2018-02-24)5th Birthday! (2018-02-25)Popular (100, ‎2018-10-30)Prolific (100, 2019-02-27)Philosopher (500, ‎2019-02-28)

Re: Failure to Export to MSC Nastran

Valued Contributor
Valued Contributor
Yes. The licensing changed between NX 11 and NX 12. NX 12 requires an additional license module for MSC Nastran export as well as Abaqus export and possibly others. We ran into this issue as well. I would suggest you contact your Siemens sales representative to come to a resolution.