Showing results for 
Search instead for 
Did you mean: 

NX-Motion and Link to components with asserted mass properties do not work


When I want to create Links in NX-Motion to model components (parts) that have set mass and inertia properties with the tool Advanced Weight Management (assert values), their mass are not considered in the calculation. Such a Link with mass property option set to "Automatic" shows always 0kg and 0 for inertia.

Yes I know that their is a "User"-mode to set the properties manually but I would like to use the predefined (precalculated) asserted values from the models and cannot find any way to do this.

Is there a solution or workarround or is it impossible?

Thanks for reading!