Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Stress Wizard - is it possible to edit mesh/loads/constraints without repeating all the steps?

Valued Contributor
Valued Contributor

Hi,

 

I have a simulation done with Stress Wizard. Is it possible to reopen it in Stress Wizard and edit (for example change the mesh size and force value)? I tried for quite a long time, and I can only create new loads and change material. I cannot however change the mesh size or load values.

I know I can edit it with 'Design' application, but it requires another license bundle. Ideally, I'd like to reopen the analysis in Stress Wizard, edit the mesh/loads/constraints and recalculate the solution without running 'Design' module at all. Is it possible?

If not, does it mean, that in Stress Wizard we can set up analysis only once and in case of changes we have to re-create it from scratch?

 

thanks in advance!

 

WZ

1 REPLY 1

Re: NX Stress Wizard - is it possible to edit mesh/loads/constraints without repeating all the steps

Siemens Legend Siemens Legend
Siemens Legend
Hi WZ,

The wizards are limited in functionality and allow a one way setup of a simulation. You cannot reopen the simulation in the Wizard. But the Wizard generates a *.fem and *.sim file that can be opened and modified in Design Simulation or Simcenter.

Best regards
Boris