Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Stress Wizzard mesh point

Experimenter
Experimenter

I would like to apply a force on point on a surface to see how a construction behaves under that load. I use the NX Stress Wizzard and can select planes and lines, however not point. I know there is a mesh point option but that seems to be only available in the Pre/After module. Since I am using a NX for Design license I don't have access to that module. Is there a way to apply the force to a point? I tried making a normal point on the surface but that disappears once the mesh is made. This is the workflow that I am following:

 

https://www.youtube.com/watch?v=AX9HzuRnIpU

1 REPLY 1
Highlighted

Re: NX Stress Wizzard mesh point

Phenom
Phenom

Can you create a very small circular "patch". The centre being the point where you want to apply your force. If you have to have a force apply to a point then using a very samll diameter will get close. This will create meshing issue potentially

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)