Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Thermal Symmetric Model

Valued Contributor
Valued Contributor

I have  a model that has symmetry, so I only meshed half of it. When I look at the nodal results I am seeing as I get to the edge of the symmtery that there is a small decrease in temperature. But when I run a full model where I have a 360 degree mesh I do not have this small decrease in temperature. Could this simply be a post processing issue?

3 REPLIES

Re: NX Thermal Symmetric Model

Gears Phenom Gears Phenom
Gears Phenom

Do you apply symmetry boundary condition like zero thermal flux?

Re: NX Thermal Symmetric Model

Siemens Phenom Siemens Phenom
Siemens Phenom

In a thermal model, a face with no boundary conditions *is* a symmetric face. In the absence of a boundary condition, a free face will have no flux in the normal direction. There are no "symmetric" boundary conditions to be applied.

Highlighted

Re: NX Thermal Symmetric Model

Valued Contributor
Valued Contributor

Contacted MAYA and was told to utilize the Radiation Periodicity option. Doing that solved the issue.