Parallel solving error in simcenter coupled flow

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

 

So i'm trying to Resimulate a coupled thermal-flow model which was done by my colleague and was successful with different parameters, but the solving gets interupted after a while (at first it was after 1 hour 15 minutes)

 

i made sure that Mpich2 is installed and i even updated to the latest version of the Thermal-Flow module (Simcenter3D_ThermalFlow_2019.1.6_svn142723_wntx64)

 

here's the first error i got before updating te Thermal-Flow moduleCapture.JPG

 

then after the update it started getting interrupted sooner

Captur2525e.JPG

 

Any idea what's causing this?

 

Thanks in Advance!

 

Helmi Bouali

1 REPLY 1

Re: Parallel solving error in simcenter coupled flow

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Helmi,

 

From the second image it seems like the solver is still pointing to a NX12 folder. Are you still running the model from NX12 with the new patch or are you now running from SC2019.1?

 

It isn't recommmended to run with the newer version of the solver with an old version of NX/Simcenter.

 

Regards,

Jean-Frédéric