Scenarios in Simcenter FEM analysis

Builder
Builder

Hello,

I would like to do in Simcenter what can be done in Solid Works (scenarios), that is to run an analysis wen a number of parameters take different values. Foe example a diameter will be 10, 20, 30 mm and a length 100, 110, 140. This will lead to a 3x3=9 scenarios.

Is it possible, but not using Journals?

Many thanks

Ionut

1 REPLY 1

Re: Scenarios in Simcenter FEM analysis

Phenom
Phenom

See the optimisation Module. One of the option is about sensitivity analysis and does (if I recall!) what you are looking for. Specific licence required however!

 

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)