Cancel
Showing results for 
Search instead for 
Did you mean: 

Solve subcase only?

Gears Valued Contributor Gears Valued Contributor
Gears Valued Contributor

Dear experts,

 

is there a way to solve only one subcase of a solution?

 

I've got two subcases right but messed up the other. After the correction of the messed up one, I do not want to solve the two correct ones again.

 

Cheers.

4 REPLIES 4

Re: Solve subcase only?

Gears Phenom Gears Phenom
Gears Phenom

You can duplicate whole analysis case and remove all subcases except one you need.

Re: Solve subcase only?

Gears Valued Contributor Gears Valued Contributor
Gears Valued Contributor

But then I have 2 result files?

A way to combine?

Re: Solve subcase only?

Siemens Legend Siemens Legend
Siemens Legend

Hello,

I think, easiest option is clone the existing solution having multiple subcase., Then in the newly created solution (by cloned) keep the subcase required and delete the unwanted one.

 

Thanks

RB

Highlighted

Re: Solve subcase only?

Gears Phenom Gears Phenom
Gears Phenom

Is this crucial?