Cancel
Showing results for 
Search instead for 
Did you mean: 

Source of MatML format files for use in NX

Gears Phenom Gears Phenom
Gears Phenom

I've looked at matweb.com and their MatML files do not comply 100% with the MatML.org schema, so they will not import into the new IMM (Integrated Material Management) tool.

 

Any know of any other sources for MatML, or VDA, CSV, BOM, or Cas format material properties?

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
5 REPLIES

Re: Source of MatML format files for use in NX

Pioneer
Pioneer

Hi everyone,

 

I would like to add that MatMl files created with NX don't work with ANSYS. They should, since MATML is supposedly a standard.

 

yours

Cyril

Re: Source of MatML format files for use in NX

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

I have read Ansys MatML files from a material library website into NX.  But I have not tried NX to Ansys. 

Re: Source of MatML format files for use in NX

Creator
Creator

Hello,

Have you exported tha ANSYS MatML file from the database MatWeb?

http://www.matweb.com

Is this working fine?

I'm looking for a material library I can import to NX.

Do you have experinence with other libraries?

 

Thanks.

 

Franz

Re: Source of MatML format files for use in NX

Legend
Legend

Funny, I was just responding to another thread about this!  Yes, the ANSYS MatML from matweb imports fine (at least in NX10)

Re: Source of MatML format files for use in NX

Creator
Creator
Thanks!
Sorry, but after I placed my thread I found this existing in the System... ;-)