Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Stress wizard simulation report does not display E Modulus

Experimenter
Experimenter

I ran the NX stress wizard on a part, upon completion it generates a simulation report (html file) showing lots of values for the material properties. Most of these values are listed as not defined or null, as is the value for Young's Modulus (E). Since I am running this stress wizard to proof to a proofing institute that the part is sound, I need to show that I have worked with the right material properties. Right now I can not show this.
When I go to Manage Library Materials I check the material via Information or Inspect I can verify it has the right values. How can I make this values appear in the final simulation report?

I am on NX 12 with an NX for Design license, so the stress wizard is my only FEM option.