TMG Fatal Error no clue of what it is

Experimenter
Experimenter

Hi,

 

I try to run a thermal analysis but I always have the same error and have no clue about how to solve it.

I search on google, here, and I even tried to reach the Hotline but it is never answering.

 

The error is the following :

 

 

Cpu time= 174.2 ECHOS Module

 

Calculating geometrical parameters...

 

** FATAL **

** Error in PUT routine, IARR= 212 IEL=********** IEL2= 1

 

 


** FATAL **

** Run aborted due to errors.

 

What surprised me is that my model already worked, I just add some elements and suppressed other but I was vigilant on modifying my constraints and simulation objects. I try to run with and without radiation, reports, etc and I always have the same fatal.

 

Thank a lot for your help

5 REPLIES 5

Re: TMG Fatal Error no clue of what it is

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

 

It is possible this is a Bug in the solver. Could you tell me which TMG version you are using? It would be at the top of the .log file.

 

Also which number did you try calling?

 

Thanks!

Jean-Frédéric

Re: TMG Fatal Error no clue of what it is

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

It seems like a weak spot in echos for larger number of elements. Please renumber your NX elements starting from 1 and give it a try again. Can you send us the model if the problem is not resolved?

Also try to update your TMG patch.

 

Mohamed SAGHIR

Re: TMG Fatal Error no clue of what it is

Experimenter
Experimenter

Hi Jean-Frédéric,

 

I'm using the TMG 12.0.0 from Sep 12 2017.

I finally managed to have someone and opened an IR. I'm waiting for more info.

 

Thanks for your help,

Clémence

Re: TMG Fatal Error no clue of what it is

Experimenter
Experimenter

Hi Mohamed,

 

I'm gonna try to renumber my elements from 1. Thank you for your advice, I'll let you know if it's working.

 

Clémence

Re: TMG Fatal Error no clue of what it is

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

TMG12.0.0 is a very old patch. In addition to renumbering your elements, I would try installing the latest patch you can download it from here, you will need a webkey account:

 

https://download.industrysoftware.automation.siemens.com/download-n.php/simcenter/Simcenter_3D_Suppo...

 

Thanks,

JF