Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Use the "view synchronize" option between 2 different FE models (*.sim)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Dear experts,

 

Is it possible to synchronize 2 FE results (based on 2 FE models --> 2 *.sim files) in the same way as with the "view synchronize" option in the result tab of Simcenter 3D?

The  "view synchronize" options can be used to synchronize 2 viewports, but based on the same *.sim file.

If I have 2 models (with only some structural changes like some thicknesses, radius, etc between the 2 models) and have generated the same stress plot for both models, is it possible or not to synchronize them in the postprocessing?

 

thank you very much

regards

Sébastien 

2 REPLIES 2

Re: Use the "view synchronize" option between 2 different FE models (*.sim)

Siemens Phenom Siemens Phenom
Siemens Phenom

View Synchronize work for me when using results from 2 different solutions in 2 different .sim files.

 

It is simply synchronizing the origin, rotation and zoom of the view, so it shouldn't care if the models in each view are the same or different..

Re: Use the "view synchronize" option between 2 different FE models (*.sim)

Siemens Experimenter Siemens Experimenter
Siemens Experimenter
Thank you for the quick answer.
Indeed the view synchronize option works with 2 different *.sim files based on regular FE results.
It was an missunderstanding as I used the new "specialist durability" and in this case if I switch the *.sim files to visualize a new durability result, the viewports with the durability results disapear.