When SImcenter Will Add "CGNS in fluid As Dipole by BEM" workflow

Creator
Creator

May I ask when the Simcenter 3D will add the workflow?  I want to solve Vibro-acoustic Problem by BEM ,but the acoustic is from CFD using dipole, but the Simcenter can only use it in the FEM,which can be done by Virtual.Lab 13.10.Normally, the new Simcenter should work better than the older "Virtual.Lab".However,it is so sad that the new Simcenter cannot support the basic function.

 

Hopefully It Will Add in Simcenter SOON,which it's an awesome software I have ever used!! IF missing the function ,what a pity.

 

Best Regards

 

Yours sincerely!