Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Writing results for certain nodes over several subcases to a external table

Valued Contributor
Valued Contributor

Hello guys,

 

I have a solution including lots of subcases. Therefore I want to check the reaction forces in x, y and z direction for the same 5 nodes in all the subcases and list them in a table. Does anybody has an idea how to perform this in NX 9.0?

 

Thank you in advance,

 

Georg

2 REPLIES

Re: Writing results for certain nodes over several subcases to a external table

Siemens Phenom Siemens Phenom
Siemens Phenom

Georg,

 

You can generate the data using the Multiple Reduction command. Specify the type to be a graph and choose the start/end load cases appropriately. Define your expression (formula) as desired from your scalar results inputs. You can then select nodes, elements, or geometry along with different averaging/combining options. If you choose no averaging options, then you will get a graph for each of the selected entities. For example if my expression is DX (X displacement component) and I select 5 nodes for 10 load cases, then I will get 5 XY graphs showing results across all of the selected load cases.

 

The graph is stored in the post processing navigator. Listing the graph will show all the data for all of the graphs. Such as:

 

Graph Title: DX
Abscissa Label:Iteration
Abscissa Unit: Number
Ordinate LabelSmiley Very HappyX
Ordinate Unit: mm

Data Format: Real Only

Record Name: At Node 4495
X Value Y Value

1. 1.000000E+000 1.967302E-002
2. 2.000000E+000 -5.700348E-005
3. 3.000000E+000 -2.042553E-001
Record Name: At Node 4546
X Value Y Value

1. 1.000000E+000 1.661525E-002
2. 2.000000E+000 -3.739967E-004
3. 3.000000E+000 -2.188557E-001
Record Name: At Node 4632
X Value Y Value

1. 1.000000E+000 9.380033E-003
2. 2.000000E+000 -1.118409E-003
3. 3.000000E+000 -2.278992E-001

 

The data can also be stored in AFU records.

 

Regards,

Mark

 

Mark Lamping

Simulation Product Management

Product Engineering Software

 

Siemens Industry Sector

Siemens Product Lifecycle Management Software Inc.

2000 Eastman Drive

Milford, OH  45150

Tel. (513) 576-2073

mark.lamping@siemens.com

Re: Writing results for certain nodes over several subcases to a external table

Siemens Phenom Siemens Phenom
Siemens Phenom

Note that NX doesn't support emoticons. I copied/pasted : next to a D. ;-)