Change post view default parameters

Pioneer
Pioneer

NX 11 - Default post view option.pngGood morning,

 

Every time I load a different result, I have to change the post view attributes of the deformation because it is too wavy with the default parameters. Would there be any way to save different default values, to customise the visualisation parameters desired? For instance, in the attached picture, I'd like to find by default "Scale 50.0 absolute" instead of "Scale 10 %model".

 

Thank you and regards,

 

Oscar

5 REPLIES 5

Re: Change post view default parameters

Phenom
Phenom

create your own post-view template !

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Change post view default parameters

Pioneer
Pioneer

Thank you for the tip. Any hint about how to create it?

Re: Change post view default parameters

Siemens Phenom Siemens Phenom
Siemens Phenom

See "Post view templates" in the online help

Re: Change post view default parameters

Pioneer
Pioneer

Thank you.

 

I've progressed quite well, but when I can't find the template editor to create a partial template:

 

NX 11 - User templates warning when right click + edit.png

 

Would you know how to proceed to enable this feature or is included only under special licenses?

 

 

Re: Change post view default parameters

Siemens Phenom Siemens Phenom
Siemens Phenom

Siemens PLM does not provide any XML editor. You can use any 3rd party editor that you like. You just need to tell NX which one to open via the UGII_CAE_POST_TEMPLATE_EDITOR variable.

 

Configure the template file XML editor

 

 

https://en.wikipedia.org/wiki/Comparison_of_XML_editors