Highlighted

Contact in Linear statics 101

Pioneer
Pioneer

I have modelled a flange connection with preloaded bolts. I gave face contact between the flange faces in contact.

I have attached the f06 file, kindly help me with the error.

4 REPLIES 4

Re: Contact in Linear statics 101

Phenom
Phenom

Have you actually checked what the SFM is "suggesting" ? May have part(s) "flying" i.e no properly constrained

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Contact in Linear statics 101

Gears Phenom Gears Phenom
Gears Phenom

Looking at the f06, it says in the warning that to contact elements are formed. Something in the preprocessing happens

Re: Contact in Linear statics 101

Phenom
Phenom

so you're contact are not set up properly or do not occur (wrong face selection for shell elements !). If you are relying on the contact to prevent rigid bodies then you have them and SOL101 crashes. Difficult to say without seeing the model

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Contact in Linear statics 101

Phenom
Phenom

Hi, read the following about contact in Sol 101 and the chapters above in online documentation. Maybe you can find the reason of your problem there.

 

Summary of Significant Aspects of Contact in Sol 101

 

Hint: Sometimes an already defined contact definition is not placed in the solution afterwards, check it, please. Best wishes, Michael

| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX12 | engelke engineering art GmbH, Germany | 2019-07-08
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution". Kick Off (2015-09-14)On the Map (2016-10-21)1st Gear 2018 (2018-02-19)5th Birthday! (2018-02-25)Popular (100, ‎2018-10-30)Prolific (100, 2019-02-27)Philosopher (500, ‎2019-02-28)Problem Solver (50, 2019-06-25)