Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Convert .AFU file into a .txt file

Valued Contributor
Valued Contributor

I am trying to open an AFU file where is contained an FRF that I previously computed in NX Nastran 12.
Is there any way to convert directly this data into a .txt or .dat files without passing from exportation in NX Nastran environment as text file?

Regards

A

1 REPLY 1

Re: Convert .AFU file into a .txt file

Siemens Phenom Siemens Phenom
Siemens Phenom

No. AFU files are binary and access is via an internal API. You would need to use NX/Simcenter (or I-deas) to read the file.

 

The attached file is a simple journal that will open an AFU and dump the data contents of each record to a csv file. Run it in NX/Simcenter via Tools, Journal, Play