Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Creating an mnf-File (SOL103) for Adams, making the von-mises-stress visibile in Adams-Postproc.

Experimenter
Experimenter

I am sucessfully creating a mnf-File importing it in Adams. The deformation is showed in the Adams-Postprocessor as I estimated it, but the von Mises-Stress is not visible.

There must be a setting in Nastran-Solver getting the stress-visibilty. I do not find it.

2 REPLIES

Re: Creating an mnf-File (SOL103) for Adams, making the von-mises-stress visibile in Adams-Postproc.

Siemens Genius Siemens Genius
Siemens Genius

Hi

OUTGSTRS =yes write grid point stress to MNF.

Did you specify  OUTGSTRS =yes  in ADAMSMNF  card ?( I think it is NO by default)

Thanks

Ramesh

Re: Creating an mnf-File (SOL103) for Adams, making the von-mises-stress visibile in Adams-Postproc.

Experimenter
Experimenter

I edited the Adams-mnf-card like this while I inserted "OUTGSTRN=YES" and "OUTGSTRS=YES":

 

MBDEXPORT ADAMS STANDARD FLEXBODY=YES FLEXONLY=NO MINVAR=PARTIAL ,
RECVROP2=YES PSETID=NONE OUTGSTRN=YES OUTGSTRS=YES

 

The rest of the parameters are set by NX.

But there was no effect in Adams.