Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Durability - How to simulate an experiment

Experimenter
Experimenter

I need to do a durability analysis, in the structure of a bike, I have to apply totally reverse forces of 600N in a position according to the image below, per 100000 cycles.

96315801-dac5-469c-a58b-3d05a1905255.jpg

 

 

Can I use SOL101 static solution? How to define the forces in order to change the direction?

 

I performed a simulation, with only a load static of 600N, in a single direction, and for cyclic function I used "Full-unit cycle". Is this right?

 

Thank you,