Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Dynamic forced response in Simcenter structure

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi, 

In the SC13500 simcenter structure package, can I perform express simulations like "forced response" (sinesweep, random) and transients (shock) ?. Through new solution type 103 Dynamic response, new event ... for example ..

 

or necessarily I need to buy the Simcenter Response Dynamics add-on (code SC30521). 

 

Could someone confirm this?, please

2 REPLIES 2

Re: Dynamic forced response in Simcenter structure

Siemens Phenom Siemens Phenom
Siemens Phenom

The SOL 103 Response Dynamics solution computes the normal modes and additional matrices required for Simcenter Response Dynamics. There are no excitations defined in a SOL 103 Response Dynamics run and no responses are computed. Simcenter Response Dynamics is required to define excitations and compute responses using the modal data ganerated by the SOL 103 Response Dynamics solution.

Re: Dynamic forced response in Simcenter structure

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks very much JimB.

 

As a Siemens´s partner, I always used a complete NX (full package), I've done some dynamic response simulations. But I am not sure if I offer to a new customer just the simcenter structure package or also add the dynamic response package.

 

Now this is clearer for me