Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Element quality criteria

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hello,

I need to do element quality control in NX12 (NX Nastran) and I have the prescribed

 

Aspect = 8
Stretch = 0.25
Jacobian = 0.5
MidPoid dev = 33.3
MidPoid alig = 33.3
UserThickness = 0.1mm
Mesh>A.Paste = 0.1mm
Check Duplicate
Check Negativ Volume

Percentage of TRIA Shell < 5%
Warping Shell: 15° Ideas
Warping Solid: 25° Ideas
Aspect Ratio Shell: 1:4
Aspect Ratio Solid Tetra: 1:8
Internal Angle QUAD: 40°-140°
Internal Angle TRIA: 20°-120°


I do not know how to find out


Stretch
MidPoid dev
MidPoid alig
UserThickness
Mesh>A.Paste

 

I think these are the element quality parameters of Catie or Abaqus.

Do not you know what quality controls in NX Nastran to assign to them?


I have no explanatory document on what the quality criteria are.

 

Antonín