Error on SOL 601/106

Pioneer
Pioneer

I am getting the below attached error when I tried to run the non-linear analysis in NX-9. Please help me to   understand the following error.

 

Thanks

1 REPLY 1

Re: Error on SOL 601/106

Siemens Phenom Siemens Phenom
Siemens Phenom

The root cause is the "Error: Temperature -253.15000 used in TABLEMk 1 does not match in TABLEST 2.

 

This means that you have a temperature dependent material (TABLEM) with temperature dependent stress-strain data (TABLEST).

 

The temperature values on both tables need to match. If your TABLEM has data at T=-253.15, then your TABLEST also needs an entry at T=-253.15 which points to a TABLES1 containing stress-strain data at that temperature.