Cancel
Showing results for 
Search instead for 
Did you mean: 

Error opening NASTRAN F06 file

Creator
Creator

Seems I have something basic not set correctly.

Solve completes without errors but I cannot  find results.

I have searched both Locally and in TeamCenter

I don't find .op2 or f06

 

Any suggestions?

5 REPLIES 5

Re: Error opening NASTRAN F06 file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

This is something to improve in NX AdvSim, the management of NX NASTRAN errors. The user only is aware that a problem exist when doing click in RESULTS > STRUCTURAL, and only then the following window will appear in screen:

 

NO-RESULTS-SET.png

 

Also, the reason why you don't find the *.f06, *.op2 files is because you forgot to save your FEM/SIM model, then go to "<nx_install_dir>/UGII" and all your nastran files will be there.

 

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/
Highlighted

Re: Error opening NASTRAN F06 file

Creator
Creator

I faild to identify the true problem actually Nx Nastran fails to solve

 

gtac helped me find that i had a known issue :  the NX9.0.3 "cinflex error"

(previously I did not have the problem with NX9.0.2)

 

To resolve the problem I modified the nast9.rcf file to supply; port@host information.

Also works if I delete the line Auth=28000@cinxflex1,28000@cinxflex2,28000@cinxflex3

seems like nastran is picking up my environment variable.

Re: Error opening NASTRAN F06 file

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Oh yes, I remember I suffered the same problem, but simply investigating the *.log file I realized of the error, it was a slip from developers!!. Happy you are OK.

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Error opening NASTRAN F06 file

Experimenter
Experimenter

how i modify the line ? i really need your answer


@lmeares wrote:

I faild to identify the true problem actually Nx Nastran fails to solve

 

gtac helped me find that i had a known issue :  the NX9.0.3 "cinflex error"

(previously I did not have the problem with NX9.0.2)

 

To resolve the problem I modified the nast9.rcf file to supply; port@host information.

Also works if I delete the line Auth=28000@cinxflex1,28000@cinxflex2,28000@cinxflex3

seems like nastran is picking up my environment variable.


 

Re: Error opening NASTRAN F06 file

Siemens Phenom Siemens Phenom
Siemens Phenom

If you have the env variable SPLM_LICENSE_SERVER defined, you only have to delete the auth= line from the .rcf file.

 

If not, youo need to change the line to auth=28000@hostname, where hostname is the name of your sites' license server.