Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export Abaqus setup with element/node sets from sim file

Experimenter
Experimenter

I'm creating an Abaqus input file from NX and would like to also export defined groups as element and node sets.

 

Is this possible ?

 

I'm using the Simcenter v11.0.2.7 Translator for Abaqus version 6.14-3

2 REPLIES 2

Re: Export Abaqus setup with element/node sets from sim file

Siemens Phenom Siemens Phenom
Siemens Phenom

This option will be available in Simcenter 2019.1. You will be able to optionally export all groups and/or selection recipies as sets.

Re: Export Abaqus setup with element/node sets from sim file

Experimenter
Experimenter
Unfortunately I cannot wait that long.

So for everyone else: I have used additional "dummy" constraints in NX to export specific element sets.