Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Export max displacements to ASCI

Builder
Builder

Hello!
 I would be really grateful if someone has advice or a solution for my problem. On the first view, the problem seems to be simple and small but until now I could not manage to do it.

I have a relatively simple model and im running a static analysis on it (sol 101). 4 Interfaces are fixed restrained and on the last interface an unit force is applied. My aim is to somehow export the max displacements in an automatable way. (Identify results -> export is not recordable unfortunately)

When I'm creating a report, a really great summarized table with the max displacements is printed in .htm. But this report has to be initialized first, which is not automatable either.

Is there a way to export the max displacements of the loadcase to an asci file like the .f06 or .pch?

I read something about the PARAM,PRTMAXIM but that does not deliver the desired results somehow (or does not change anything in the output files).

There's also the possibility to export ALL displacements to the punchfile. I could postprocess all the displacements and look for the max displacement, but I am not sure if this is not exaggerated for such a "simple" problem.

 

Thank you in advance

 

Kind regards

Benny

 

4 REPLIES

Re: Export max displacements to ASCI

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

Insert in the nastran bulk data PARAM,PRTMAXIM,YES and you will have written in the F06 file the maximum results.

 

0                                                  MAXIMUM  SPCFORCES       
  SUBCASE/
  DAREA ID        T1             T2             T3             R1             R2             R3
0        1   1.4334236E+03  1.8182344E+04  1.0423561E+04  0.0000000E+00  0.0000000E+00  0.0000000E+00
0                                                  MAXIMUM  DISPLACEMENTS   
  SUBCASE/
  DAREA ID        T1             T2             T3             R1             R2             R3
0        1   1.1411084E-01  3.1414744E-01  4.5617911E-01  0.0000000E+00  0.0000000E+00  0.0000000E+00
0                                                  MAXIMUM  APPLIED LOADS   
  SUBCASE/
  DAREA ID        T1             T2             T3             R1             R2             R3
0        1   7.1428599E+03  0.0000000E+00  1.4285710E+04  0.0000000E+00  0.0000000E+00  0.0000000E+00

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Export max displacements to ASCI

Builder
Builder

Thank you for your fast answer!

Unfortunately, I can't find this kind of results in my .f06 file although I activated prtmaxim.

 

Here is my input file

$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
NASTRAN ELEMITER=YES
NASTRAN ITER=YES
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
$* FILE MANAGEMENT
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
$* EXECUTIVE CONTROL
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
ID,NASTRAN,input_sim1
SOL 101
CEND
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
$* CASE CONTROL
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
ECHO = NONE
SPC = 100
OUTPUT
DISPLACEMENT(PLOT,REAL) = ALL
$*  NX Step: Radial
SUBCASE 1
LABEL = Radial
LOAD = 3
$*  NX Step: Axial
SUBCASE 2
LABEL = Axial
LOAD = 4
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
$* BULK DATA
$*
$*$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$$
$*
BEGIN BULK
$*
$* PARAM CARDS
$*
PARAM     EXTOUT DMIGPCH
PARAM        F56     YES
PARAM      K6ROT100.0000
PARAM     OIBULK     YES
PARAM    OMACHPR     YES
PARAM       POST      -2
PARAM    POSTEXT     YES
PARAM   PRTMAXIM     YES
PARAM    UNITSYS   MN-MM
$*
$* GRID CARDS

 

Re: Export max displacements to ASCI

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hello!,

The reason is because you are using the ITERATIVE SOLVER, not the DIRECT SPARSE SOLVER. Desactivate the iterative solver in the study definition and you will have written for sure the maximum results in the F06 file, OK?.

Best regards,

Blas.

Blas Molero Hidalgo, Ingeniero Industrial, Director
IBERISA • 48004 BILBAO (SPAIN)
WEB: http://www.iberisa.com
Blog Femap-NX Nastran: http://iberisa.wordpress.com/

Re: Export max displacements to ASCI

Builder
Builder

Thank you very very much! It works! You saved me so much work