Re: How to specify viscoelastic material property in Nx?!

Genius
Genius

Thank you @HYK, I would like to model a simple SDOF model with elastomer connected to the ground and an aluminium mass.

Then extract the Frequency Response Function (FRF) in Z direction on the aluminium mass (with a resonance damped by the elastomer loss factor). SDOF elastomer.PNG

 

 

 

I attached a simple FEM model (but incomplete: the elastomer model is not defined as well as the solution to extract the FRF). Can someone help me to create the proper setup?

 

I attached in a excel the material properties of the elastomer in terms of complex shear modulus (G*)  over the frequency range also depited below. Consider Poisson = 0.49, hence E*(omega)=3 x G*(omega).
Elastomer.png

 Regards,

A