Cancel
Showing results for 
Search instead for 
Did you mean: 

Missing temperature pre-load in NX 10

Creator
Creator

Hi all,

 

I am currently using NX 10. I have noticed that the Nastran Temperature Pre-load feature is missing in the Solution Step as compared to older NX versions. May I know if this feature has been removed or has it been relabelled as another function?

 

Best regards,

Gregory

4 REPLIES 4

Re: Missing temperature pre-load in NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

Prior to NX 10, temperature specification was spread out over 7 different areas:

 

  1. Temperature loads in the solution Loads container
      --> Exported to TEMP bulk referenced by TEMP(LOAD) in the Global Case
  2. Initial Temperatures Default on Solution/General Tab
      --> Exported to TEMPD bulk referenced by TEMP(INIT) in the Global Case
  3. Material Temperatures Default on Solution/General Tab
      --> Exported to TEMPD bulk referenced by TEMP(Material) in the Global Case
  4. Temperature Load Default on Solution/General Tab
      --> Exported to TEMPD bulk referenced by TEMP(LOAD) in the Global Case
  5. Temperature Pre-Load loads on Solution/Pre-Load Conditions Tab
      --> Exported to TEMP bulk referenced by TEMP(LOAD) in the each Solution Step
      --> Note also that this is a load, not a pre-load
  6. Initial Temperatures Simulation Object
      --> Exported to TEMP bulk referenced by TEMP(INIT) in the Global Case
  7. Material Temperatures Simulation Object
      --> Exported to TEMP bulk referenced by TEMP(Material) in the Global Case

On Export, temperatures in all 3 TEMP(LOAD) are globbed into one SID. Temperatures in both TEMP(INIT) are globbed into a second SID. Temperatures in both TEMP(MATERIAL) are globbed into a third SID

 

 

This was all cleaned up in NX 10. All temperature specification is now done via a Temperature Set:

 

NewTempSet.png

 

A Temperature Set definition consists of a type (Initial, Load, Material), a label, a description and a default temperature value:

 

 TempSetDialog.png

 

 The Type and Label correspond directly to the case control entry (i.e. TEMP(INIT)=1 or TEMP(LOAD)=101). The default temperature becomes the bulk data TEMPD card for that SID.

 

Once the set is created, multiple temperature loads can be added to the set.

 

NewTempLoad.png

 

All temperature loads are defined via a single Temperature Load dialog

 

 TempLoadDialog.png

 

Re: Missing temperature pre-load in NX 10

Creator
Creator

Hi JimB,

 

Thanks for your detailed explanation. You are a great help to me.

 

Thank you!

 

Best regards,

Gregory

Re: Missing temperature pre-load in NX 10

Experimenter
Experimenter

Hello,

 

Thanks for the explaination.

But I have a question.

In NX5 (yes long ago Smiley Wink) I tesedt a temperature load on a beam

clamped in both ends, so I could verify the stresses with the

coefficients with thermal expansion.

 

The only thing I had to do (if i recall correctly) was put on a temperature load
eg 300 degrees and define somewhere the normal temperature.

 

I would like to do this again in NX10 (OK first a metal and then a Laminate).

But I am confused of the possible options nowadays and the temperature
seems not to appear as a load in the navigator.

 

What I want is to indicate that the stress free state temperature is 20 degrees
and that the current temperature is 200 degrees.

 

Thanks for your time,

 

Regards,

 

Olaf

Highlighted

Re: Missing temperature pre-load in NX 10

Siemens Phenom Siemens Phenom
Siemens Phenom

First, it's generally not good forum etiquette to reopen a 9 month old thread. In the future, create a new post and reference the old one if needed.

 

Second, I'm not sure I can post a more detailed reply now than the one posted last year. If you want to specify an isothermal temperature difference, you simply need to create a temperature set of type Initial/Stress Free and set the default temperature value of that set to T1. Then create a second temperature set of type Load and set the default temperature value of that set to T2. Your delta T will then be T2-T1.