Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Nastran Design simulation analysis

Experimenter
Experimenter

Hello guys,

 

I am currently struggeling with a problem. I have some simulations running on NX Nastran in NX11. The Simulations are working perfectly. But my problem starts with the analysis of them. In order to compare some of the results to  the actual real workpiece I wanted to create some defined points on the structure of the piece. NX should then give me back the displacement of these Points. I could then compare the displacement that was calculated by the simulation with the displacement of the same points at the real part.
Do you have any idea how I could achieve this or even better a simpler way on how I could compare my simulation results with the workpiece in the real world?

 

Thank you in advance for your appreciated answers!!!

 

Best regards

 

Till

1 REPLY 1

Re: NX Nastran Design simulation analysis

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor
Moved the post to Simcenter > CAE Simulation - NX Nastran Forum > NX Nastran Design simulation analysis

Cheers, Ben