NX Nastran Not Running

Experimenter
Experimenter

Hello,

 

I was recently moved to a new machine at work. When I tried running a simulation, the FEA program did not run.

Attached is the error I am given. It says, "Although no NX Nastran fatal errors were detected, no results were created.
Please review the NX Nastran logs for information on the cause of this problem." When I look to the logs, all three are empty (log, f04, f06).

Interestingly enough, when I run a study created on another laptop, that study will run just fine. If I edit the study, it will revert to display the previous analysis and disregard the changes.

I checked the licenses between my old computer and the new one, but everything seemed in order.

 

Any help would be greatly appreciated.

3 REPLIES 3

Re: NX Nastran Not Running

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Try launch batch cases on NX Nastran

run cmd as an administrator

 

For example - such as my file paths

C:\>PLM\NX11\NXNASTRAN\bin\nastran64.exe C:\NXTEMP\trubka_sim1-solution_1.dat mem=200000000 parallel=4

 

Of course you can add additional commandline options (e.g. mem=..., parallel=...). The list of available Nastran commandline Options can be found in the documentation or by starting Nastran with the commandline option "help all".

 

*.F04 *.F06 *.log *.op2 - you ca see in the root

 

For example - C:\>trubka_sim1-solution_1.log

 

Do you see anything?

Re: NX Nastran Not Running

Experimenter
Experimenter

This is what pops up. Looking through the files that were created, the only one I can see as problematic is the .f06 file. Here's the part that seems problematic.

 

*** USER WARNING MESSAGE 333 (GETLIN)
THE BEGIN BULK STATEMENT IS MISSING. A BEGIN BULK STATEMENT WILL BE INSERTED BY THE PROGRAM
1 OCTOBER 6, 2017 NX NASTRAN 8/25/13 PAGE 1

0 N A S T R A N F I L E A N D S Y S T E M P A R A M E T E R E C H O
0


NASTRAN BUFFSIZE=8193 $(C:/PROGRAM FILES/SOLID EDGE ST8/SIMULATION/X64/NASTRAN/C
NASTRAN DIAGA=128 DIAGB=0 $(C:/PROGRAM FILES/SOLID EDGE ST8/SIMULATION/X64/NASTR
NASTRAN PARALLEL=4 $(COMMAND LINE[3])
NASTRAN REAL=2147483647 $(PROGRAM DEFAULT)
1 OCTOBER 6, 2017 NX NASTRAN 8/25/13 PAGE 2

0 N A S T R A N E X E C U T I V E C O N T R O L E C H O
0


||||||
*** USER FATAL MESSAGE 505 (XCSA)
CONTROL CARD IS ILLEGAL
CEND $ GENERATED BY GETLIN
1 * * * END OF JOB * * *


*** USER WARNING MESSAGE 1153 (XCLNUP)
THE NDDL FOR THIS DATA BASE HAS NEITHER BEEN CREATED NOR OBTAINED FROM THE DELIVERY DATA BASE.
USER INFORMATION: THE DATA BASE CREATED IN THIS RUN IS TOO IMMATURE TO BE RESTARTED.
USER ACTION: DELETE THIS DATA BASE BEFORE STARTING YOUR NEXT RUN.

Re: NX Nastran Not Running

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi,
can you share the .dat file?

 

*** USER FATAL MESSAGE 505 (XCSA)

CONTROL CARD %1 IS ILLEGAL

User information:

The statement preceding Message 505 cannot be processed correctly.

This message

may also be issued if an invalid character; such as a

control character appears on the statement.