Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX Nastran solving on a server?

Honored Contributor
Honored Contributor

Is it possible to solve on a server type computer, instead of the local workstation?  ie stup the job locally, and queue it up on a server machine?

 

if so, what are the hardware reqts for the server?  os? anything else we need to be aware of?

-Dave
NX 11 | Teamcenter 11 | Windows 10
3 REPLIES

Re: NX Nastran solving on a server?

Siemens Phenom Siemens Phenom
Siemens Phenom

Yes, this is possible. That is the difference between the desktop/bundle licenses and the Enterprise license.

 

If solving with a desktop/bundle license, the solve must be on the same machine that the deck was exported from Simcenter on (i.e. local solve)

 

To solve on any machine other than the one that the deck was exported on, an enterprise license is required.

Re: NX Nastran solving on a server?

Experimenter
Experimenter

Jim,

 

I need to do network server solves as well to offload NASTRAN jobs for a large group of NX users (have Enterprise install). 

 

Please can you provide links or info on how to setup?

What job schedulers are supported?

 

Thanks,

 

Mark.

Re: NX Nastran solving on a server?

Siemens Phenom Siemens Phenom
Siemens Phenom

Siemens PLM does not directly support remote job queueing.

 

There are several partners that provide queing solutions (i.e. Platform Computing LSF, PBS pro, GRD)