Cancel
Showing results for 
Search instead for 
Did you mean: 

Nastran Results Format

Experimenter
Experimenter

Hi,

Im trying to simulate thermal problem by using SOL 601,106 (advanced nonlinear statics) by introducing initial temperature and temperature load variables. It should be direct set up. But no result file appear and the message came out : "no result file found ".

 

Im requesting output requst of displacement and stress value. In FO6. file, it says that no FO6. file defined eventhough i already created one. The other message in fo6.file as below :

 

   *** New internal database created.
     ***WARNING: Case control SPC is specified, but no SPC set is defined.
     ***ERROR: PID 2000234 is not found.
 *** Allocating 8188 MB of memory ...
 
 *** FATAL ERROR: PROCESSING OF NASTRAN DATA FOR SOL 601 FAILED.
 *** ADVANCED NONLINEAR EXIT CODE 0 ***
 *** ISHELL PROGRAM 'NXNA' COMPLETED ***
 ^^^ USER FATAL MESSAGE 
 ^^^ ERROR IN ADVANCED NONLINEAR MODULE          0
 ^^^SOL601 FAILED 

 

Any ideas that could be trigger to solve this issue?

 

Regards,

Sarah

1 REPLY 1

Re: Nastran Results Format

Siemens Phenom Siemens Phenom
Siemens Phenom

There are 2 relevant lines in the text posted:

 

     ***WARNING: Case control SPC is specified, but no SPC set is defined.

     ***ERROR: PID 2000234 is not found.

 

The first is a warning. It means that there is a SPC request in case control (i.e. SPC = 10), but there are no SPC* cards in the bulk data with this SID (10). This is a warning - meaning that the solution will continue without the SPC's

 

The second is the error. Somewhere in the deck there is an element that points to PID 2000234, but there is no corresponding property card (PSOLID, PSHELL, etc.) with that ID. Since properties are not defined for element(s), the solution cannot continue.