Highlighted

Plotting Across Iterations

Experimenter
Experimenter

Hi,

 

I have 77 load cases. I want to plot the variation in stress at a single node over these load cases. I thought that the way to do this would be to right click on the post view node -> New Graph -> change Graph Type to Across Iterations. However, the only option I have for Graph Type is On Path. I have attached a screenshot as an example. How can I access the Across Iterations graph type? Do I have the right method for accomplishing what I wish to do?

 

I am using NX 8, and have performed a Linear Statics solve. Thanks in advance.

 

noAcrossIterations.png

 

Cheers