Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Question about using TSTEPNL

Pioneer
Pioneer

Hello everybody. I am new here.

 

My question is how do I get NX Nastran to use the TSTEPNL modeling object/card in case control?

 

I am trying to perform a SOL601,129 solution and in the Solution Attributes --> Case Control --> Time Step Intervals - it doesn't let me select the nonlinear transient parameter (TSTEPNL) for that, so how do I make that happen?

 

Is the TSTEPNL card "required" for SOL601,129 or will the TSTEP card suffice?

 

Any help in this would be greatly appreciated.

 

Thank you.

2 REPLIES 2

Re: Question about using TSTEPNL

Siemens Phenom Siemens Phenom
Siemens Phenom

TSTEPNL is not supported in Advanced Nonlinear (SOLs 601,x or 701). See Remark 15 here:

https://docs.plm.automation.siemens.com/tdoc/nxnastran/11/help#uid:index_QRG:id512196:id510921:id511...

 

And the description here ("TSTEPNL is intended for SOLs 129 and 159"):

 

https://docs.plm.automation.siemens.com/tdoc/nxnastran/11/help#uid:index_QRG:id511876:id509346

 

Note that SOL 129 <> SOL 601,129

Re: Question about using TSTEPNL

Pioneer
Pioneer

Ahhh...okay.

 

That explains it then.

 

Thank you.