Highlighted

Restart and DBCLEAN

Pioneer
Pioneer

Hello,

 

I am performing a Read-Only restart and am getting the following warning on the .f06 output file. There are no fatal messages but I would like to know if it is a best practice to use the DBCLEAN statement while performing read-only restarts.

 

Capture.JPG

 

 

Thank you,

Sam

 

2 REPLIES 2

Re: Restart and DBCLEAN

Phenom
Phenom

how have you defined the restart parameters?

DBCLEAN is ignored because there is nothing to clean it seems?

Production: NX.CAE 10.0.2.6
Development: VB.NET (amateur level !)

Re: Restart and DBCLEAN

Pioneer
Pioneer

Hi,

 

I have defined a Read-only Restart following the example below:

image.png

I don't see where I should define a version ID or Project ID

 

Thanks,

Sam